Part Number: AM2732
Other Parts Discussed in Thread: AWR2243,
Hello,TI's engineer:
We have a question about HWA memory.Let me give you a practical example.
We use two AWR2243 and one AM2732 to develop cascade radar.Each HWA memory band is 16K.
If ID-FFT out result is 16K,then we should do 2D-FFT,the input of 2D-FFT data size is 16K,and M0 is sufficient for this memory.However the output of 2D-FFT data size is 32K,the M2 is not sufficient for this memory.What should we do in this situation?Because the memory addresses of M2 and M3 are contiguous,will additional 16KB be automatically put into M3?
BR
Bryant