Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Using tivaware_c_series_2_1_4_178 with the EK-TM4C1294XL LaunchPad I have the TIRTOS (tirtos_tivac_2_16_00_08) example "tcpEcho" building and once running I get the following in the output display window.
CORTEX_M4_0: ss in flash
Starting the TCP Echo example
System provider is set to SysMin. Halt the target to view any SysMin co
CORTEX_M4_0: ntents in ROV.
CORTEX_M4_0: Service Status: DHCPC : Enabled : : 000
CORTEX_M4_0: Service Status: DHCPC : Enabled : Running : 000
CORTEX_M4_0: Network Added: If-1:10.177.20.152
CORTEX_M4_0: Service Status: DHCPC : Enabled : Running : 017
When I try to communicate with the TM4C1294XL hardware using the application "tcpSendRceive.exe" I receive the following.
C:\TI\tirtos_tivac_2_16_00_08\packages\examples\tools>tcpSendReceive 1:10.177.20.152 1000 1 -s100
getaddrinfo failed: 11001
Am I using the correct IP address? What do I need to do to get the communications working?