This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1105: Eval Brd needed

Part Number: MSPM0G1105
Other Parts Discussed in Thread: MSPM0G3507, MSPM0G1106

I am looking for an Eval Board for the MSPM0G1105. Can you suggest an eval board I can replace the IC with the MSPM0G1105 in the 48-VQFN package? 

Best,

Gina

  • Hi Gina,

    We don't have evaluation boards for each device and every package, but we do have evaluation boards for the MSPM0G3507 which is in the same family.

    LP-MSPM0G3507

    This board is good for MSPM0G1106, when you're doing evaluation the extra features the G3507 has is the analog (DAC, COMP, Zero-drift OPAs), CAN interface, and a bit more memory. If you don't use any of the analog or the CAN interface then you can do a bulk of your development on this launchpad. Also pay attention to the pins you're utilizing as this launchpad is using the 64 pin package.

    Regards,
    Luke