Part Number: MSPM0L1306-Q1
Other Parts Discussed in Thread: SYSCONFIG
1. 用MSPM0L1306-Q1 (VSSOP 28封装)做了一个板子,现在可以开机和运行LED闪烁程序。
2. 正在debug PWM out的程序,用PA14(TIMG1, C0)输出,但是始终没有在示波器上看到PWM波,查过示波器设置没有问题。
3. 下面是PWM的初始化程序,麻烦查一下,看看是哪里的问题,谢谢!
#define GPIO_PWM_PORT (GPIOA)
#define GPIO_RGB_PWMOUTT_PIN (DL_GPIO_PIN_14)
#define GPIO_IOMUX_RGB_PWMOUTT (IOMUX_PINCM15)
#define GPIO_IOMUX_FUNC_PWMOUTT_PWM (IOMUX_PINCM15_PF_TIMG1_CCP0)
static const DL_TimerG_ClockConfig gLIGHTSENSOR_PWM_OUTT_INSTClockConfig = {
.clockSel = DL_TIMER_CLOCK_LFCLK,
.divideRatio = DL_TIMER_CLOCK_DIVIDE_1,
.prescale = 0,
};
static const DL_TimerG_PWMConfig gLIGHTSENSOR_PWM_OUTT_INSTConfig = {
.period = RGB_LED_PERIOD, /* 64Hz PWM signal for visible light */
.pwmMode = DL_TIMER_PWM_MODE_EDGE_ALIGN,
.startTimer = false,
};
void PWMout1_init(void)
{
DL_GPIO_initDigitalOutput(GPIO_IOMUX_RGB_PWMOUTT);
DL_GPIO_clearPins(GPIO_PWM_PORT, GPIO_RGB_PWMOUTT_PIN);
DL_GPIO_enableOutput(GPIO_PWM_PORT, GPIO_RGB_PWMOUTT_PIN);
DL_GPIO_initPeripheralOutputFunction(GPIO_IOMUX_RGB_PWMOUTT, GPIO_IOMUX_FUNC_PWMOUTT_PWM);
///========================================
DL_TimerG_setClockConfig(LIGHTSENSOR_PWM_OUT_INST,
(DL_TimerG_ClockConfig *) &gLIGHTSENSOR_PWM_OUTT_INSTClockConfig);
DL_TimerG_initPWMMode(LIGHTSENSOR_PWM_OUT_INST,
(DL_TimerG_PWMConfig *) &gLIGHTSENSOR_PWM_OUTT_INSTConfig);
/* Configure 50% duty cycle */
DL_TimerG_setCaptureCompareValue(
LIGHTSENSOR_PWM_OUT_INST, PWM_OUTT_PERIOD / 2, DL_TIMER_CC_1_INDEX);
DL_TimerG_clearInterruptStatus(
LIGHTSENSOR_PWM_OUT_INST, DL_TIMER_INTERRUPT_ZERO_EVENT);
DL_TimerG_enableInterrupt(
LIGHTSENSOR_PWM_OUT_INST, DL_TIMER_INTERRUPT_ZERO_EVENT);
DL_TimerG_enableClock(LIGHTSENSOR_PWM_OUT_INST);
DL_TimerG_setCCPDirection(LIGHTSENSOR_PWM_OUT_INST, DL_TIMER_CC1_OUTPUT);
DL_TimerG_startCounter(LIGHTSENSOR_PWM_OUT_INST);
}