Part Number: MSPM0L1306
Hello,
I see this note on the TRM which states that if the BSL pin is asserted when the MSPM0 comes out of SHUTDOWN, then the device will enter BSL:

But in the example we use, PA18 is the switch to wake up from Shutdown and it does not appear to force the device into BSL (LEDs continue blinking to indicate wakeup count). However, if I wake up the device from the button PA18 this does not happen.
Is there some sort of override in the BSL or wakeup logic which prevents BSL entry in the case where the wakeup pin is the same as the BSL pin?
Munan