This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I want to use a RTOS on a TMS570LS1224. I took a look at FreeRTOS and ThreadX wich provides ports for the Cortex-R4F. In the context save and restore functions the registers r0 to r15 are handled and in case the FPU is active also the registers d0 to d15. I wonder why the registers S0 to S31 does not need to be preserved during a context switch?
What is the prefered way to detect if the FPU is active and the FPU registers have to be preserved therefore?
Kind regards
Jens
Hi Jens,
Can you please refer below thread once, this might be useful in this context:
--
Thanks & Regards,
Jagadish.