Part Number: AM2634
Hi BU,
I am asking this for my customer and need your official confirmation:
In customer's application, there are configuring RTI timer's input clk source as WUCPUCLK, configuring SYSCLK 200MHz and ADC CLK prescaler to input clock/4.0, i.e. 50MHz. Is this configuration ok for AM263x? Especially, is 50MHz ok for ADC module, because the max frequency of ADC is 50MHz, it is an edge value. They want to confirm with TI that the above clk configuration are always worked under whole temperature range.
Regards,
Will