Part Number: TMS570LC4357
Hi,
I tried to load UDP example on to the dev kit (TMS570), I get following error. (I did not do any changes to the project)
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR5: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
CortexR5: File Loader: Verification failed: Values at address 0xF0407FF0 do not match Please verify target memory and memory map.
CortexR5: GEL: File: C:\Users\...\2110.Hercules_Ethernet_Bootloader_UDP\Hercules_Ethernet_Bootloader\TMS570LC43x\Build-TMS570LC43x\Debug\Build-TMS570LC43x-tftpBoot.out: a data verification error occurred, file load failed.
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
2110.Hercules_Ethernet_Bootloader.zip
--
I had to disable verification step to load this project on to the dev kit.
Can you please advise what is wrong with the project?
Regards,
Abhi