Hi,
Is it possible to use SPIs in main domain from M4F in FFI island in the case of Safety support device ?
My customer wants use up to 6ch SPIs by M4F, but only two SPIs in MCU island. Non-safe SPI is OK for 4ch of 6ch SPIs.
Regards,
Hideaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to use SPIs in main domain from M4F in FFI island in the case of Safety support device ?
My customer wants use up to 6ch SPIs by M4F, but only two SPIs in MCU island. Non-safe SPI is OK for 4ch of 6ch SPIs.
Regards,
Hideaki
Hello Hideaki,
I have gone through your question.
I know your question is if main/SoC_SPIs can be used from MCU Domain in FFI island.
Can you help in referring me to a document customer is using to know about FFI Island?
My customer wants use up to 6ch SPIs by M4F, but only two SPIs in MCU island. Non-safe SPI is OK for 4ch of 6ch SPIs.
I need help in understanding the line you wrote above.
Please clarify the following questions:
1. How many MAIN Domain SPIs are going to be used by MCU Domain.
2. How many MCU Domain SPIs are going to be used by MAIN Domain.
Regards,
Vaibhav
Hi Vaibhav,
Thanks for your reply and apologies in my late response.
The customer wants to use 6ch SPIs by M4F as Safety MCU in MCU domain (isolated FFI Island).
However, the datasheet describes that there are only 2ch SPI in MCU domain, but 5ch SPI in Main domain.
Therefore, they’re considering to have M4F use also 4ch SPI in Main domain.
Can M4F can access these SPI in Main domain in the case of Isolated FFI mode ?
1. 4ch Main domain SPIs are going to be used by M4F in MCU domain.
2ch MCU domain SPIs are going to be used by M4F in MCU domain.
2. R5F in Main domain doesn’t use SPI.
Thanks and regards,
Hideaki
Hi Hideaki,
Thanks for your response.
As far as the timeout gasket is configured/available for the SPI peripheral, the safety core can access Main Domain SPI channel in case of Isolated FFI mode.
I am also going to assign this thread to a safety expert to help you with this thread.
Thanks for your patience.
Regards,
Vaibhav