Part Number: MSPM0G3507

Why is this error displayed after I move the contents of adc12_internal_temp_sensor_mathacl_LP_MSPM0G3507_nortos_ticlang into an empty file? I didn't change any code, I did the same configuration
Thank you !
In addition, what is _iqQ15? How to use it? Is there a more accurate advantage in ADC conversion? The voltage collected by my ADC is much worse than the actual voltage, which causes me to be very inaccurate in the measurement of resistance, inductance, and other devices. Is there any solution
Finally, I would like to ask why I cannot see the value of the defined variable during debugging, and even the variable type can only be displayed unknown. Only when I use Volatile can I observe the value of the variable. When I debug, I step by step, and local variables also cannot see the value when entering the function. And I can't set breakpoints for some sentences. Why?
There are many questions. Thank you very much for your help!!!