Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: MCU_OSC0_XI和MCU_OSC0_XO电平

Part Number: AM2432
Other Parts Discussed in Thread: AM2434

Hi  AM2432 :

   In section 7.7.3 of the manual for am2432, it is shown that the VIH should be greater than 0.65 * VDDS-OSC. However, during my actual testing, the signal amplitude of the MCU OSC0_XI pin input was 1.02V, which is lower than the required VIH amplitude in the manual, but it does not affect the normal operation of am2432. I would like to know why the input signal of MCU OSC0_XI is not 1.8V.

     Note:

     Crystal frequency: 25MHz
     Crystal load capacitance: 33pF