Part Number: MSPM0L1106
Other Parts Discussed in Thread: LP-MSPM0L1306
Hello
I would like to operate a MSPM0L1106 (SOT-23-THN (DYY)) on a SOT23-16 breakout board as a target on a LP-MSPM0L1306 LaunchPad. On the breakout board, all 16 pins are directly connected to the microcontroller.
If I remove all connections between XDS110-ET and MSPML1306 and connect the connections directly to the corresponding pins on the breakout board (schema Launchpad => MSPM0L1106 SOT-23-THN as shown below)
is it then possible to program the MSPM0L1106 via the LaunchPad?
GND => VSS
5 V => NC
3V3 => VDD
RXD => PA22
TXD => PA23
NRST => PA1
SWDIO => PA19
SWCLK => PA20
BSL => PA18