This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: AM2634

Part Number: AM2634

Good morning, for the development of a project we would like to develop code through the automatic generation of code made available by embedded coder (matworks ambient). Are there any libraries for the R2 family (2634 in particular) that I can download and use for automatic code generation? Does this tread mention your availability?

Greetings.

  • Hello Andrea Canestrari,

    MATLAB model-based design flow and automated code generation (Embedded Coder Hardware Support Package) for AM263x is under development. 

    Early Access release will be available tentatively by end of April 2024 with following features. We will post the instructions/links for downloading the package when available.

    • Target/HSP definition (AM263x ControlCard)
    • Toolchain: TI ARM CLANG
    • Target features – Scheduling
    • Application deployment
    • OS: Baremetal (timer based scheduler)
    • Single core support
    • Peripheral device driver blocks – GPIO, HWI, UART, ADC, EPWM

    Thanks

    K.Sanjeev