Part Number: TMS570LC4357
I try to make TMS570LC4357 bootloader. I act as follows, but it occur prefetchEntry Error when I jump to APP_START_ADDRESS(0x00200100).
1. my bootloader Code based on TI example
2. I use sciReg3 communication. I test write bin with ymodem.
3. After the download, I jump to APP_START_ADDRESS(0x00200100). Which project is made with same project and start address shift.
4. when i jump to addr0x00200100 : prefetchEntry error is occurred.
The jump addr code as follows,
JumpAddress = (uint32_t)(APP_START_ADDRESS);
((void (*)(void))JumpAddress)();
I found that the error is happening only with RTOS Code. if its a BareMetal code working fine . when the OS Start Scheduler called that time only my code is not running. if required i can share my both application code and Bootloader code For reference. the same Application code which i commented the OS Start Scheduler Part and it is running Fine. I think this issues is due to the Vector table Mapping.
I checked the forum and found the following post; I tried the same with my bootloader but received the same error.
feel free to connect with me .
Regards,
Mr.K