Part Number: MSP432E401Y
Hi experts,
i'm looking for an analog switch IC to switch between the circuits..
For example,
My input has 64 pins, circuit number 1 which has 64 pins and circuit number 2 has also 64 pins..
so i need to give 64 pin input to circuit number 1 for sometime and for some time i need to give input for the 2nd circuit..
Also some times i need to connect input pins to both circuits at a time..
Do we have that type of analog switch I C please let me know if it ?
i'm thinking to implement 64channel sp3t analog switch IC (i don't know whether this this type of switch is there or not), Any thoughts on this ?
Best regards,
Tex