Part Number: MCU-PLUS-SDK-AM243X
Hello,
my AM243X-EVM stopped working from one day to the next day.
I always followed the startup-procedure, having the power switch to off, connecting the power source, the debugger and then turn the power on. so far all LEDS are going green. I also always follow the description in the documentation for EVM DEV-Boot by setting boot-pins to DEV-Boot-mode, like described in the picture. When I then try executing the script like it is described I run into this error:
This is new and never happened before. I did not change the target configuration in the meanwhile or anything else. it just stopped when I started it up another day. A manual connect just shows shortly the 0x00000024 and then it restarts automatically after some seconds and I can't reconnect at all, always showing the DAP-access-error:
The board itself is probably not populated with an hs-fs-sitara but with an gp-sitara since it was sealed at 09/08/22 but nevertheless it did work that way before. But also if I try to do it the old way with the no-boot mode it doesn't work. it won't even read out the boot mode correctly and always tells me the boot mode is 0x00.
A repower leads to the same behaviour all the time. I also restarted CCS, my PC, made everything powerless, disconnected and reconnected everything. the debugger, the power-cable of the evm, each one for itself, all together.... but the problem persists. A colleaguw also had this issue out of nowhere and we weren't able to fix this.
How can I solve this problem?
Best regards
Felix