Part Number: AM2431
Hi Team
We are using AM2431 in our design, we have shortlisted the PSRAMs with both 3.3V and 1.8V supply voltage to interface with the MCU. During the Noise margin analysis we came to know that all those PSRAMs are failing since the VOH(min) margin is less for the MCU. Need your thoughts here.
Can you please suggest any PSRAMs with parallel interface which can be interfaced with AM2431 MCU.
| SL/NO | SOURCE | DESTINATION | Check status | |||||||||||||||
| PART | Supply Voltage Rail | Supply Voltage(V) | VOH(MIN) | VOH(MAX) | VOL(MIN) | VOL(MAX) | PART | Supply Voltage Rail | Supply Voltage (V) | VIH(MIN) | VIH(MAX) | VIL(MIN) | VIL(MAX) | Supply Voltage | High Volatge Level | Low Voltage Level | STATUS | |
| 1 | AM2431BSDFHIALVR | 1V8 | 1.8 | 1.35 | 1.8 | 0 | 0.45 | AS1C8M16PL-70BIN | 1V8 | 1.8 | 1.4 | 2 | -0.2 | 0.4 | TRUE | FALSE | FALSE | NOT OK |
| 2 | AM2431BSDFHIALVR | 1V8 | 1.8 | 1.35 | 1.8 | 0 | 0.4 | IS66WVE4M16EBLL-70BLI | 1V8 | 1.8 | 1.4 | 2 | -0.2 | 0.4 | TRUE | FALSE | TRUE | NOT OK |
| 3 | AM2431BSDFHIALVR | 3v3 | 3.3 | 2.4 | 3.3 | 0 | 0.4 | IS67WVE4M16EBLL-70BLA1 | 3V3 | 3.3 | 2.9 | 3.5 | -0.2 | 0.4 | TRUE | FALSE | TRUE | NOT OK |
Regards
A V S