Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD263: Ethernet Port Configuration For RGMII Interface

Part Number: TMDSCNCD263

Hello Team,

we are using Eth, Port and EthTrcv driver from MCAL_AM263x_09.00.01.00 package, we are trying to create autosar Ethernet stack.

when we are trying use RGMII1 port from the TMDSCNCD263 PROC110A board, we are not able to see ethernet communication on the bus, but from our software side all initialization is successful and  tries call Eth_transmit successfully everytime. we are using Polling mode and not interrupt for Rx and Tx.

Is there any additional settings that we need to take care with respect to Jumper settings, Port , Eth and EthTrcv configuration.

Also can you please provide us the sample demo configuration for the below shown RGMII interface

Please find attached configurations for Eth, Ethtrcv and Port and let us know the changes that we need to take care.

Also we reffered the sample files shared as part of Package (\mcal\examples_config) but still we have issue in setting up communication.

Eth_Configurations.zip

Regards,

Pradeep R