Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0G3507: M0G3507230903261

Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3507

Hello TI Community!

I am working with the MSPM0G3507 microcontroller and using the CCS Theia development environment. I need to set the microcontroller to operate at its maximum clock frequency of 80MHz to optimize the performance of peripherals such as timers, comparators, and ADCs. However, I am struggling to find this option in the CCS Theia interface. Could someone guide me on how to access and configure this functionality? Specifically, I'm looking for the option to adjust the system clock to the maximum frequency allowed by the microcontroller.

Any help or guidance on where I can find these settings in the CCS Theia interface would be greatly appreciated. Thank you for your help!