This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: CAN interrupt data adquisition

Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN

Im starting a proyect with can interruptions,

/** @file sys_main.c 
*   @brief Application main file
*   @date 11-Dec-2018
*   @version 04.07.01
*
*   This file contains an empty main function,
*   which can be used for the application.
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com 
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* Includes */
#include "system.h"
#include "spi.h"
#include "het.h"
#include "gio.h"
#include "reg_pcr.h"
#include "sys_pcr.h"
#include "sys_pmm.h"
#include "reg_vim.h"
#include "sci.h"
#include "string.h"
#include "reg_can.h"
#include "can.h"
#include "sys_common.h"
#include "sys_core.h"
#include "sys_vim.h"
#include "reg_mibspi.h"
#include "reg_can.h"
#include "adc.h"
#include "i2c.h"
/* USER CODE END */

/* Include Files */

#include "sys_common.h"

/* USER CODE BEGIN (1) */
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
/* Globals */
typedef struct qMessage
{
    uint8_t     len, sciRxMessage, rxData;
    uint8_t     buffer[128];
} qMessage_t;

typedef struct qMessage3
{
    uint32_t    id;
    uint8_t     buffer[8];
    uint8_t     interface;
}xMessage3;


void sysInit(void);
void canTest(void);

/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */
    sysInit();
    canTest();
    while(1);
/* USER CODE END */

    return 0;
}


/* USER CODE BEGIN (4) */

void canTest()
{
//    uint32_t canId;
//    xMessage3 *rxCanMessage = NULL;

    sciSend(scilinREG, 34, (unsigned char *)"\r\n********************************");
    sciSend(scilinREG, 34, (unsigned char *)"\r\n**********  CAN test  **********");
    sciSend(scilinREG, 34, (unsigned char *)"\r\n********************************");
    sciSend(scilinREG, 2,  (unsigned char *)"\r\n");
    sciSend(scilinREG, 12, (unsigned char *)"\r\nDeveloper:");
    sciSend(scilinREG, 24, (unsigned char *)"\r\n           Marco Mecha");
    sciSend(scilinREG, 2,  (unsigned char *)"\r\n");

    static uint8_t data[8] = {0x03, 0x0A, 0x03, 0x0A, 0x0B, 0x0C, 0x0B, 0x0A};

    if (canTransmit(canREG3, canMESSAGE_BOX1, data)){
        sciSend(scilinREG, 22,  (unsigned char *)"\r\nData send via can: ");
        sciDisplayData(scilinREG, data, 8);
        sciSend(scilinREG, 2,  (unsigned char *)"\r\n");
    }
//    while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX2) || !canIsRxMessageArrived(canREG3, canMESSAGE_BOX2));
//    sciDisplayData(scilinREG, rxCanMessage->buffer, 8);
//    sciSend(scilinREG, 2,  (unsigned char *)"\r\n");
//    sciSend(scilinREG, 2, rxCanMessage->buffer);

}


void sysInit()
{
    uint8_t generic = 0;
    sciInit();                                      //SCI initialization.
    canInit();                                      //CAN initialization.

    //Enable interrupts:
    _enable_interrupt_();                           //General interrupt flag.
    //Enable GIO interrupt:
    //Enable SCI interrupt:
    sciEnableNotification(scilinREG,SCI_RX_INT);    //Enable SCI Lin interrupt by Rx.
    sciEnableNotification(sciREG,SCI_RX_INT);       //Enable SCI interrupt by Rx.
    //Enable CAN interrupt:
    canEnableErrorNotification(canREG2);            //Enable canREG2 interrupt.
    canEnableErrorNotification(canREG3);            //Enable canREG3 interrupt.
    //Enable I2C interrupt:
    //i2cEnableNotification(i2cREG1, I2C_RX_INT);
    //i2cDisableNotification(i2cREG1, I2C_RX_INT);

    sciReceive(scilinREG,1, (unsigned char *)&generic);
    //sciReceive(sciREG,1, (unsigned char *)&generic);    //We have to set interuptions and execute this instruction to use the SCI
    //i2cReceive(i2cREG1, 1, (unsigned char *)&generic);

    //sciDisableNotification(sciREG,SCI_RX_INT);       //Disable SCI interrupt by Rx.

    sciSend(scilinREG, 37, (unsigned char *)"Initializing system. Please wait...\r\n");
    gioInit();                                      //GIO module initialization.
    gioSetDirection(hetPORT1, 1 << 15);             //Enable N2HET1[15] as output. This is the output signal to the external watch-dog.
    gioSetDirection(spiPORT3, 0x11);                //to set the SPI3NCS[0] to output direction. The SPI3NCS[0] is the bit0 of SPIPC1 register.
                                                    //to set the SPI3NCS[4] to output direction. The SPI3NCS[4] is the bit4 of SPIPC1 register.
    gioSetDirection(mibspiPORT5, 0 <<9);
    gioSetDirection(mibspiPORT1, 0 <<1);

    //By default we set the GIO pins for long test as follows:

    gioSetDirection(mibspiPORT1, (0 << 9));         //Set MibSPI1_CLK direction. This is the bit 9 in the SPIPC3 register.
    gioSetDirection(gioPORTA, (0 << 6));            //Set GIOA[6] direction. This is the bit 6 of GIODIRA register.
    gioSetDirection(mibspiPORT1, (1 << 11));        //Set MibSPI1_SOMI[0] direction. This is the bit 11 in the SPIPC3 register.
    gioSetDirection(mibspiPORT1, (1 << 10));        //Set MibSPI1_SIMO[0] direction. This is the bit 10 in the SPIPC3 register.
    gioSetBit(mibspiPORT1, 10, 0);                  //We set the GIOs as logic 0
    gioSetBit(mibspiPORT1, 11, 0);                  //We set the GIOs as logic 0


    gioSetBit(spiPORT3, 0, 1);                      //Disable External memories SPI communication
    gioSetBit(spiPORT3, 4, 1);                      //Disable External memories SPI communication

    sciSend(scilinREG, 27, (unsigned char *)"\t************************\r\n");
    sciSend(scilinREG, 27, (unsigned char *)"\tLabOSat-02 [OBC] OS V1.0\r\n");
    sciSend(scilinREG, 27, (unsigned char *)"\t************************\r\n");
    sciSend(scilinREG, 1, (unsigned char *)"\n");
    sciSend(scilinREG, 14, (unsigned char *)"Developers: \r\n");
    sciSend(scilinREG, 30, (unsigned char *)"\t Gagliardi Leandro Luciano \r\n");
    sciSend(scilinREG, 22, (unsigned char *)"\t Di Nardo Federico \r\n");
    sciSend(scilinREG, 1, (unsigned char *)"\n");
}

/*********************************
 * SCI interrupt service routine *
 *********************************/
void sciNotification(sciBASE_t *sci, unsigned flags)
{
    uint8_t *rxKey = NULL;
    if(sci == scilinREG){
        sciReceive(scilinREG, 1, rxKey);
        sciSend(sci, sizeof(uint8_t), rxKey);
    }
}

/*********************************
 * CAN interrupt service routine *
 *********************************/

void canMessageNotification(canBASE_t *node, uint32 messageBox)
{

    xMessage3 *rxCanMessage;

    while(!canIsRxMessageArrived(node, canMESSAGE_BOX2));

    rxCanMessage->id = canGetID(node, messageBox);
    canGetData(node, messageBox, rxCanMessage->buffer); /* copy to RAM */

    sciSend(scilinREG, 22,  (unsigned char *)"\r\nData reciv via can: ");
    sciDisplayData(scilinREG, rxCanMessage->buffer, 8);
    sciSend(scilinREG, 2,  (unsigned char *)"\r\n");

}


/* USER CODE END */

Im getting as ouput in the UART 

Data reciv via can: FFFFFEEAFFFFFEEA
Data send via can: 030A030A0B0C0B0A

when im expecting the results to be the same.

Running in debbug mode also doesn't show the  rxCanMessage change.

I also tried using a global variable but the results where the same.

Thanks in advance, Marco Mecha