This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: EtherCAT subdevice buffer handling API receives wrong bit sizes in callbacks

Part Number: AM2434

Hi there,

I have another problem with EtherCAT Subdevice Stack and Buffer Handling API.
I am using:

- EtherCAT Subdevice Stack from TI/Kunbus
- Industrial Communications SDK 09.01. release

I am using following stack functions to regsiter callbacks
    EC_API_SLV_cbRegisterPreSeqInputPDBuffer(...);
    EC_API_SLV_cbRegisterPostSeqInputPDBuffer(...);
    EC_API_SLV_cbRegisterPreSeqOutputPDBuffer(...);
    EC_API_SLV_cbRegisterPostSeqOutputPDBuffer(...);

However, these callbacks do not get the correct bit lengths. The bit lengths seem to be interchanged. I get the bitlength of OutputPDBuffer in InputPDBuffer callback and vice versa.

I reproduced this behavior with the 09_01_00_00_ethercat_slave_simple_demo_am243x-evm_r5fss0-0_freertos_ti-arm-clang example. I added another RX-Pdo with 32-Bit size. After this I have RX-PDO size (96 bit) and TX-PDO size (64 bit).

I also  modify data in function registered by EC_API_SLV_cbRegisterPreSeqInputPDBuffer(...) Therefore I can be sure that the InputPDBuffer-callback is supposed to ask for data we send to SPS, as I successfully receive it in SPS. Nevertheless, the given size is wrong. In InputPDBuffer-callback I get bit size 96 bit.

See also the following patch, which clearly shows what I changed in example:

diff --git a/ecSlvSimple.c b/ecSlvSimple.c
index 7670305..319c19b 100644
--- a/ecSlvSimple.c
+++ b/ecSlvSimple.c
@@ -2146,6 +2146,36 @@ static EC_API_EError_t EC_SLV_APP_SS_populateRxPDO(EC_SLV_APP_SS_Application_t*
         goto Exit;
     }
 
+    EC_API_SLV_Pdo_t* ptRxPdo1602 = NULL;
+
+    error = (EC_API_EError_t)EC_API_SLV_PDO_create(ptSlave, "RxPDO3", 0x1602, &ptRxPdo1602);
+    if (error != EC_API_eERR_NONE)
+    {
+        OSAL_printf("Create PDO 0x1601 Error code: 0x%08x\r\n", error);
+        /* @cppcheck_justify{misra-c2012-15.1} goto is used to assure single point of exit */
+        /* cppcheck-suppress misra-c2012-15.1 */
+        goto Exit;
+    }
+    OSAL_printf("RxPDO created 0x1602: 0x%lx\r\n", (uint32_t)ptRxPdo1602);
+
+    error = (EC_API_EError_t)EC_API_SLV_CoE_getObjectEntry(ptSlave, 0x2000, 1, &ptObjEntry);
+    if (error != EC_API_eERR_NONE)
+    {
+        OSAL_printf("%s:%d Variable Error code: 0x%08x\r\n", __func__, __LINE__, error);
+        /* @cppcheck_justify{misra-c2012-15.1} goto is used to assure single point of exit */
+        /* cppcheck-suppress misra-c2012-15.1 */
+        goto Exit;
+    }
+
+    error = (EC_API_EError_t)EC_API_SLV_PDO_createEntry(ptSlave, ptRxPdo1602, "SubIndex 001", ptObjEntry);
+    if (error != EC_API_eERR_NONE)
+    {
+        OSAL_printf("%s:%d Variable Error code: 0x%08x\r\n", __func__, __LINE__, error);
+        /* @cppcheck_justify{misra-c2012-15.1} goto is used to assure single point of exit */
+        /* cppcheck-suppress misra-c2012-15.1 */
+        goto Exit;
+    }
+
     error = EC_API_eERR_NONE;
 Exit:
     return error;
@@ -2930,6 +2960,48 @@ static bool EC_SLV_APP_EoE_SS_receiveHandler(void* pContext_p, uint16_t* pData_p
     return true;
 }
 
+static uint8_t data_tx[1024]={0};
+
+static void*acquireTxBuffer(void* pContext_p, uint32_t length_p)
+{
+    static int counter = 0;
+    if(counter >> 8)
+    {
+        OSAL_printf("tx length: %d\r\n", length_p);
+        counter = 0;
+    }
+    counter++;
+
+    data_tx[0]++;
+    data_tx[1]++;
+    data_tx[2]++;
+    data_tx[3]++;
+    return &data_tx[0];
+}
+
+static void releaseTxBuffer(void* pContext_p, void* pData_p, uint32_t length_p)
+{
+    // nothing to do here just a test
+}
+
+static uint8_t data_rx[1024]={0};
+
+static void*acquireRxBuffer(void* pContext_p, uint32_t length_p)
+{
+    static int counter = 0;
+    if(counter >> 7)
+    {
+        OSAL_printf("rx length: %d\r\n", length_p);
+        counter = 0;
+    }
+    return &data_rx[0];
+}
+
+static void releaseRxBuffer(void* pContext_p, void* pData_p, uint32_t length_p)
+{
+    // nothing to do here just a test
+}
+
 /*!
  *  <!-- Description: -->
  *
@@ -3067,6 +3139,7 @@ void EC_SLV_APP_SS_applicationInit(EC_SLV_APP_SS_Application_t *pAppInstance_p)
     }
 
     /*PDO Mapping Changes*/
+    EC_API_SLV_PDO_setAssignment(pAppInstance_p->ptEcSlvApi, true);
     EC_API_SLV_PDO_registerAssignmentChanges(pAppInstance_p->ptEcSlvApi, EC_SLAVE_APP_assignmentChangedHandler, pAppInstance_p);
     EC_API_SLV_PDO_registerMappingChanges(pAppInstance_p->ptEcSlvApi, EC_SLAVE_APP_mappingChangedHandler, pAppInstance_p);
 
@@ -3088,7 +3161,9 @@ void EC_SLV_APP_SS_applicationInit(EC_SLV_APP_SS_Application_t *pAppInstance_p)
     EC_API_SLV_DIAG_enable(pAppInstance_p->ptEcSlvApi);
 
 #if !(defined DPRAM_REMOTE) && !(defined FBTL_REMOTE) && !(defined OSAL_FREERTOS_JACINTO) /* first omit flash */
-    EC_API_SLV_cbRegisterFlashInit              (pAppInstance_p->ptEcSlvApi, EC_SLV_APP_EEP_initFlash, pAppInstance_p->ptEcSlvApi);
+    // currently not supported for our custom board
+
+    // EC_API_SLV_cbRegisterFlashInit              (pAppInstance_p->ptEcSlvApi, EC_SLV_APP_EEP_initFlash, pAppInstance_p->ptEcSlvApi);
     /* @cppcheck_justify{misra-c2012-11.6} void cast required for signature */
     /* cppcheck-suppress misra-c2012-11.6 */
     EC_API_SLV_EEPROM_cbRegisterWrite           (pAppInstance_p->ptEcSlvApi,   EC_SLV_APP_EEP_writeEeprom, OSPIFLASH_APP_STARTMAGIC);
@@ -3098,6 +3173,12 @@ void EC_SLV_APP_SS_applicationInit(EC_SLV_APP_SS_Application_t *pAppInstance_p)
 #endif
     EC_API_SLV_cbRegisterUserApplicationRun     (pAppInstance_p->ptEcSlvApi, EC_SLV_APP_SS_applicationRun, pAppInstance_p);
 
+    /* buffer callbacks */
+    EC_API_SLV_cbRegisterPreSeqInputPDBuffer(pAppInstance_p->ptEcSlvApi, acquireTxBuffer, pAppInstance_p->ptEcSlvApi);
+    EC_API_SLV_cbRegisterPostSeqInputPDBuffer(pAppInstance_p->ptEcSlvApi, releaseTxBuffer, pAppInstance_p->ptEcSlvApi);
+    EC_API_SLV_cbRegisterPreSeqOutputPDBuffer(pAppInstance_p->ptEcSlvApi, acquireRxBuffer, pAppInstance_p->ptEcSlvApi);
+    EC_API_SLV_cbRegisterPostSeqOutputPDBuffer(pAppInstance_p->ptEcSlvApi, releaseRxBuffer, pAppInstance_p->ptEcSlvApi);
+
     error = (EC_API_EError_t)EC_API_SLV_init(pAppInstance_p->ptEcSlvApi);
     if (error != EC_API_eERR_NONE)
     {
@@ -3350,6 +3431,9 @@ static void EC_SLV_APP_SS_applicationRun(void* pAppCtxt_p)
             }
 
 #if !(defined FBTL_REMOTE) || (0 == FBTL_REMOTE)
+#if 0
+            // I don't use this code, as processdata is updated via callbacks only
+
             err = (EC_API_EError_t)EC_API_SLV_PDO_setEntryData(pApplicationInstace->ptEcSlvApi
                     ,pApplicationInstace->ptTxPdo1A00
                     ,1
@@ -3359,6 +3443,7 @@ static void EC_SLV_APP_SS_applicationRun(void* pAppCtxt_p)
             {
                 OSAL_printf("Fill Description Object Error code: 0x%08x\r\n", err);
             }
+#endif
 #endif
         }
         else
@@ -3394,6 +3479,9 @@ static void EC_SLV_APP_SS_applicationRun(void* pAppCtxt_p)
                     lastLed = (lastLed << 1u);
                 }
 
+#if 0
+                // I don't use this code, as processdata is updated via callbacks only
+
                 //Write Led data to the process data. It can be seen in OBD in Object 0x2002:2 as well.
                 error = EC_API_SLV_PDO_setEntryData(
                         pApplicationInstace->ptEcSlvApi,
@@ -3406,6 +3494,7 @@ static void EC_SLV_APP_SS_applicationRun(void* pAppCtxt_p)
                 {
                     OSAL_printf("%s:%d:E=0x%x\r\n", __func__, __LINE__, error);
                 }
+#endif
             }
         }
 


PS: I suppose the following is true:

- Input data => Data sent from Subdevice -> SPS
- Output data => Data sent from SPS -> Subdevice
- Input data == TX data
- Output data == RX data