Other Parts Discussed in Thread: USB-TO-GPIO2
can not read the IC at Fusion Design Online
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
can not read the IC at Fusion Design Online
Hi Luo,
Do you happen to be using a USB-TO-GPIO2 adapter to read your device? Does the screen say - "Cannot find adapter" or "Cannot find device"?
Any additional information or screenshots would be helpful to help debug.
Best,
Dhanya
启动Fusion Digital Designer 界面
Launch Fusion Digital Designer interface

单击Change Device Scaning Option 界面如下:
Click on the Change Device Scanning Option interface as follows:

选择0X01 下拉菜单
Select 0X01 dropdown menu

这里面没有TPS53667选项
这里怎么操作
There is no TPS53667 option available here
How to operate here
Hi Luo,
Based on your previous responses, if my understanding is correct, you are using the adapter for power only? I believe you would have to connect the communication signals to it for the laptop to be able to detect your device.
Best,
Dhanya Prem
Hi, Luo,
For TPS53667, you will use DEVICE_CODE (MFR_44, FCh) as scan mode. For future references, if you don't know which options to choose, select the combination of "IC_DEVICE_ID + DEVICE_ID + DEVICE_CODE".
Regards
Anne Ngo
Texas Instruments
Look like GUI cannot detect adapter. Please make sure that the LED is green. If GUI does not detect Adapter, unplug the USB adapter and re-plug it in. If it still does not work, try another USB port.

Anne Ngo
Texas Instruments