Part Number: TM4C1294KCPDT
Hello,
We are using the TM4C1294 EPI interface in General Purpose Mode to interface with FPGA. In the datasheet section 11.4.4, it mentions "The configuration allows for choice of an output clock (free-running or gated), a framing signal (with frame size), a ready input (to stretch transactions), an address (of varying sizes), and data (of varying sizes)." Based on this statement it looks that the General Purpose Mode can support Ready input . However I cannot find this Ready description in either "Table 11-12. EPI General-Purpose Signal Connections" or timing picture. Can you please confirm if this Ready is supported in EPI General-Purpose Signal mode or not. If supported, could you please provide the mapped pin and timing?
Thanks,
George