This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634-Q1: XCMP example

Part Number: AM2634-Q1
Other Parts Discussed in Thread: AM2634, SYSCONFIG

Hi Champ,

From TRM , AM2634 is type5 PWM which with XCMP Submodule.

My customer found when enable the XCMP in the sysconfig, and config like below , the Counter Compare(CC ) and Action Qualifier(AQ)module still work.

But from the sysconfig below, it i should not work when enable EPWM XCMP mode.

May i know the XCMP  work in sysconfig or not?

May i know when we can have XCMP sysconfig example project?

  • Hi Huihuang,

    XCMP features are actually currently not supported by the AM263x hardware.

    I'll file a bug to reflect the same in the TRM.

    XCMP support and examples are planned to be added to AM263x devices in future.

    As of now, the AM263Px devices do support the XCMP features, if that's an alternative you would like to use.

    Regards,
    Akshit