Part Number: MSPM0L1306
I am trying to program an external MSPM0L1306 (SOT-23-THN (DYY)) with an LP-MSPM0L1306 LaunchPad.
The MSPM0L1306 is located on a breadboard, all connections of the Jumper Isolation Block J101 are disconnected and led out to the breadboard.
MSP0L1306 in the SOT-23-THN version offers 16 pins.
I tried the following mapping, but could not connect the MSP0L1306 via CodeComposerStudio 12.6.0:
Jumper Isolation Block (J101) <-> MSP0L1306
===========================================
GND <-> 6 (VSS)
5V not connected
3V3 <-> 5 (VDD)
RXD <-> 13 (PA22)
TXT <-> 14 (PA23)
NRST <-> 4 (NRST)
SWDIO <-> 11 (PA19)
SWCLK <-> 12 (PA20)
BSL <-> 10 (PA18)
What is the correct mapping of the pins from the MSPM0L1306 (unprogrammed, out of the box) to the connections of the jumper isolation block (J101)
so that the external MSP0L1306 can be connected and programmed via CodeComposerStudio 12.6.0?
Translated with DeepL.com (free version)