This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-TMS57004: LAUNCHXL-TMS57004 - (Error -242 @ 0x0) A router subpath could not be accessed. and (Error -1170 @ 0x0) Unable to access the DAP

Part Number: LAUNCHXL-TMS57004

Hello,

I'm working with a TI: LaunchXL-TMS57004, and the next day that I try to test my code, I have the next errors: 

(Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 12.6.0.00029)

(Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 12.6.0.00029)

Softwares: Code Composer Studio and Hal Code Generator.

The test connection is: 

[Start: Texas Instruments XDS100v2 USB Debug Probe]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\cynth\AppData\Local\TEXASI~1\CCS\
ccs1260\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Dec 6 2023'.
The library build time was '17:33:10'.
The library package version is '12.6.0.00029'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[The log-file for the JTAG TCLK output generated from the PLL]----------

There is no hardware for programming the JTAG TCLK frequency.

-----[Measure the source and frequency of the final JTAG TCLKR input]--------

There is no hardware for measuring the JTAG TCLK frequency.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 64 32-bit words.

The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 6 bits.

The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.

-----[Perform the Integrity scan-test on the JTAG IR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Test 1 Word 32: scanned out 0xFFFFFFFF and scanned in 0x001FFFFF.
Test 1 Word 33: scanned out 0xFFFFFFFF and scanned in 0x00000000.
Test 1 Word 34: scanned out 0xFFFFFFFF and scanned in 0x00000000.
Test 1 Word 35: scanned out 0xFFFFFFFF and scanned in 0x00000000.
Test 1 Word 36: scanned out 0xFFFFFFFF and scanned in 0x00000000.
Test 1 Word 37: scanned out 0xFFFFFFFF and scanned in 0x00000000.
Test 1 Word 38: scanned out 0xFFFFFFFF and scanned in 0x00000000.
Test 1 Word 39: scanned out 0xFFFFFFFF and scanned in 0x00000000.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 1, skipped: 0, failed: 1
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 1
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 2
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 3
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 4
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 5
Some of the values were corrupted - 73.7 percent.

The JTAG IR Integrity scan-test has failed.

-----[Perform the Integrity scan-test on the JTAG DR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Test 3 Word 0: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 1: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 2: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 3: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 4: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 5: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 6: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
Test 3 Word 7: scanned out 0xFE03E0E2 and scanned in 0x7F01F071.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 3, skipped: 0, failed: 1
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 2
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 3
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 4
Some of the values were corrupted - 65.6 percent.

The JTAG DR Integrity scan-test has failed.

[End: Texas Instruments XDS100v2 USB Debug Probe]

The card die? :( 

Please help!

  • Hello Cynthia,

    Error-1170: This is usually caused by either a hardware failure on the board or invalid code on the MCU flash that causes it to reset itself continuously. Have you programmed any code to the flash before? If it is caused by the invalid code, please try this procedure to let CPU enter a debug state:

    1. Open the target configuration window, and launch the selected the configuration
    2. Switch to debug window.
    3. Press the reset (nRST) button and hold it.
    4. Click “Connect Target” immediately after you release the nRST button.
    5. The board should be connected after couple tries.

    --
    Thanks & regards,
    Jagadish.