Part Number: AM2732
Other Parts Discussed in Thread: UNIFLASH
First of all, the chip is powered on in the uart mode. The serial assistant shows that the chip sends out two 'C' at a time. The cycle is about 4s.
Then I compiled helloworld, sbl_uart_uniflash, sbl_qspi in the sdk, and then downloaded it.
Parsing config file ...
Parsing config file ... SUCCESS. Found 3 command(s) !!!
Executing command 1 of 3 ...
Found flash writer ... sending sbl_prebuilt/am273x-evm/sbl_uart_uniflash.release.tiimage
Sending sbl_prebuilt/am273x-evm/sbl_uart_uniflash.release.tiimage: 2%|▉ | 1029/53161 [00:01<01:34, 549.22bytes/s]send error: expected ACK; got b'C' for block 1
Sent flashwriter sbl_prebuilt/am273x-evm/sbl_uart_uniflash.release.tiimage of size 53161 bytes in 6.58s.
Executing command 2 of 3 ...
Command arguments : --file=sbl_prebuilt/am273x-evm/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
Sending sbl_prebuilt/am273x-evm/sbl_qspi.release.tiimage: 0%|
what the problem is?