Part Number: AM263P4
Hello,
Some friends and I are evaluating the use of AM263x for an application and we noticed the preproduction AM263P4, which would be much more advantageous because we feel 2MB SRAM might be insufficient for our application while 3MB would be much less riskier.
- Is there any planned release date for the AM263P4?
- Will it and the AM263x be pin compatible?
- Will it be released already with the AEC-Q100 qualification?
- What would be the recommended way to connect an external RAM to it (or the base AM263x)? Would it be the GPMC?
- What is the data width of the GPMC? According to the datasheet (and to its pin description?) it is up to 16 bits but the reference manual states "8-, 16- or 32-bit-wide data path to external memory device"
Thanks,
Ricardo