Part Number: MSP432E401Y
Hi TI!!!
I need to increase the flash memory through an external 1M flash memory chip. What is the best way to do it?
Thanks very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E401Y
Hi TI!!!
I need to increase the flash memory through an external 1M flash memory chip. What is the best way to do it?
Thanks very much!
Hi,
If you have a parallel flash then you can use the EPI interface in Host Bus mode to interface with a NOR Flash memory. Refer to the EPI chapter in the device datasheet. Note that there is no hardware command write support for Flash memory devices; the Host Bus mode should only be used for Flash memory devices programmed at manufacturing time. If a Flash memory device must be written and does not support a direct programming model, the command mechanism must be performed in software.