Part Number: MSPM0L1306
Hello,
I'm using the MSPM0L1306TDGS20R with a DC/DC boost converter at 3.3V to supply the device's VDD pin. As is typical with DC/DC converters, it can be a bit noisy. I'm doing ADC conversions on an NTC thermistor and would really like to have 3.3V as the ADC reference, but I think that the noise on this supply is affecting the ADC results. I had the idea to take the 3.3V supply from the boost, RC filter it, and feed it to the VREF+ pin on the MCU. But I don't know what bias current goes into this pin (and how it might vary over time or ADC operation). I'd need this info to choose the R value in my RC filter.
Or maybe doing it this way, i.e., not having an active buffer into the VREF+ pin, is just a bad idea from the start.
Any words of wisdom appreciated.
Thanks, Randy