Part Number: AM2732
Other Parts Discussed in Thread: SYSCONFIG
I would like to interface between CPU and FPGA via MIBSPI as fast as possible.
However I don't understand exactly in CCS sysconfiguration.
- Clock Frequency (default 5000000) -> can I increase 25000000 with maximum?
- Pin Mode (4 Pin Mode with CS ) -> is it possible to configure as CLK, CS, 8bit MISO, 8bit MOSI?
If it possible, how can I configure in sysconfig of CCS ?
( I had seen only four IOs in CCS )