Part Number: MSPM0G3107-Q1
hello,
i have one question about the I/O pin
As shown in the figure below, Mcu's I/O port is equipped with a clamp diode
1)I want to know if I/O will be damaged when there is forward overvoltage and reverse overvoltage at the I/O port?
If it will cause I/O damage, Is damage caused by overcurrent? Overcurrent caused by high voltage?
2)another question: When I apply an AD port, Should I connect R2, resistors in series in the AD acquisition circuit?
please help check this follow AD acquisition circuit ,and the VIN input Power is 13.5V, Is there a problem with the circuit?My software sampling cycle is every 2ms
How do I set the values of R2 and C2 value,please help explain in details.
thank you
best regards