Part Number: TM4C123GH6PM
Ima using the driver of tivac4m123g6pm in the eeprom section I have a small issue that the funtion that writes and reads from the eeprom takes a parmeter an array of unsigned intgers but i wanted to change it to take array of floats or may be doubles or even array of character and then convert it to floats lates i tried to adjust the function in the driver to do that but it was so hard for me(getting hard fault handler or the array is not rread) and i cant do that also i used chta gpt but also it doesnt help me so could any one give me another driver or a function to use it .
iam working on a gps project and i want to save my array of latitudes and array of longitudes in the eeprom and they must be floats not intgers
here is my test function
#include <stdbool.h>
#include <stdint.h>
#include "hw_flash.h"
#include "hw_ints.h"
#include "hw_sysctl.h"
#include "hw_types.h"
#include "debug.h"
#include "flash.h"
#include "interrupt.h"
#include "sysctl.h"
#include "eeprom.h"
#include "hw_eeprom.h"
int main()
{
float latRead[8];
float lat[8] = {
110235,
112348,
115012,
118322,
121521,
124732,
127945,
130015
};
EEPROMInit();
EEPROMMassErase();
//EEPROMRead(latRead, 0x0, sizeof(latRead));
EEPROMProgram(lat, 0x0, sizeof(lat));
EEPROMRead(latRead, 0x0, sizeof(latRead));
while(1)
{
}
}
thank you,