Part Number: TMS570LC4357
Hello, how do generate two synchronous sine wave? The synchronous sine signals I want to produce must be in the 0-2V range and 4.5Khz frequency. Is it possible for me to do this? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Hello, how do generate two synchronous sine wave? The synchronous sine signals I want to produce must be in the 0-2V range and 4.5Khz frequency. Is it possible for me to do this? Thanks
İt must be Analog signal, Sine wave must be produced at voltage between -5v and +5v. Can generated negative voltage? İf possible, please explain the configuration.
Hi Furkan,
Please refer below application note to understand the sinewave generation from PWM:
Sine Wave Generation Using PWM With Hercules N2HET and HTU
--
Thanks & Regards,
Jagadish.
I understand but this cant generate negative voltage. Only above the 0V. The signal range is -5V and +5V
Hi Furkan,
I think, definitely we can't generate negative sine wave from controller.
I never tried before but after you are generating the sinewave using above app note then you should need to use a level shifter externally.
--
Thanks & regards,
Jagadish.
Well, Is there a ic that produces negative sine waves?
All controllers in general produces positive sine-waves only. You should need to contact analog team to find whether there was any level shifter IC's to convert the sinewave into positive and negative half.