Part Number: MSP432E401Y
Hi:
I have a product that uses an MSP432E401Y processor to communicate via ethernet to a network with a Netgear LB1120 4G LTE Modem. I have also been communicating using the same ethernet port with a local PC using a USB-to-Network adapter for testing and to develop new features.
I recently discovered that the latest versions of my applications no longer work when I try to communicate with the local PC. They still work fine over the Netgear LB1120.
Earlier versions of my application still work with the local PC so I must have made a change that caused this problem, but I'm having a hard time figuring out that is.
First, I tried copying code from my earlier versions to the latest version to see if I could isolate the issue and then I tried copying code from my latest version to the earlier version and each time I ran into problems.
Can anyone give me an idea of what I should be looking at to see why the connection through the USB-to-Network adapter to the local PC stopped working?
Thank you