I would like to flash my program to the flash memory and to run my application program.
Actually I don't need SBL. I just want to execute my application program.
If the SBL is need to run program, Should I do the coding for SBL ?
Then should I make me understood about the SBL and the detailed ?
Please let me know the method to run my program from flash memory.
When I try to make the example project of the SDK, it result an error.
- project name: sbl_qspi_am273x-evm_r5fss0-0_nortos_ti-arm-clang
- error name: makefile_ccs_bootimage_gen:65: recipe for target 'all' failed
then contents of this file is as next
# # Auto generated makefile # # Below variables need to be defined outside this file or via command line # - MCU_PLUS_SDK_PATH # - PROFILE # - CG_TOOL_ROOT # - OUTNAME # - CCS_INSTALL_DIR # - CCS_IDE_MODE CCS_PATH=$(CCS_INSTALL_DIR) include $(MCU_PLUS_SDK_PATH)/imports.mak include $(MCU_PLUS_SDK_PATH)/devconfig/devconfig.mak STRIP=$(CG_TOOL_ROOT)/bin/tiarmstrip OBJCOPY=$(CG_TOOL_ROOT)/bin/tiarmobjcopy ifeq ($(OS), Windows_NT) PYTHON=python else PYTHON=python3 endif OUTFILE=$(PROFILE)/$(OUTNAME).out BOOTIMAGE_PATH=$(abspath ${PROFILE}) BOOTIMAGE_NAME_GP:=$(BOOTIMAGE_PATH)/$(OUTNAME).tiimage BOOTIMAGE_NAME_HS:=sbl_qspi.$(PROFILE).hs.tiimage BOOTIMAGE_NAME_HS_FS:=sbl_qspi.$(PROFILE).hs_fs.tiimage ifeq ($(DEVICE_TYPE),HS) BOOTIMAGE_NAME=$(BOOTIMAGE_NAME_HS) else BOOTIMAGE_NAME=$(BOOTIMAGE_NAME_GP) endif BOOTIMAGE_BIN_NAME:=$(BOOTIMAGE_PATH)/$(OUTNAME).bin # # Generation of boot image which can be loaded by ROM Boot Loader (RBL) # ifeq ($(OS),Windows_NT) EXE_EXT=.exe endif ifeq ($(OS),Windows_NT) BOOTIMAGE_CERT_GEN_CMD=powershell -executionpolicy unrestricted -command $(MCU_PLUS_SDK_PATH)/tools/boot/signing/x509CertificateGen.ps1 else BOOTIMAGE_CERT_GEN_CMD=$(MCU_PLUS_SDK_PATH)/tools/boot/signing/x509CertificateGen.sh endif BOOTIMAGE_TEMP_OUT_FILE=$(PROFILE)/temp_stdout_$(PROFILE).txt ifeq ($(DEVICE_TYPE),HS) BOOTIMAGE_CERT_KEY=$(APP_SIGNING_KEY) else BOOTIMAGE_CERT_KEY=$(MCU_PLUS_SDK_PATH)/tools/boot/signing/mcu_gpkey.pem endif BOOTIMAGE_CERT_GEN_CMD=$(PYTHON) $(MCU_PLUS_SDK_PATH)/tools/boot/signing/mcu_rom_image_gen.py SBL_RUN_ADDRESS=0x10200000 SBL_PREBUILT_PATH=$(MCU_PLUS_SDK_PATH)/tools/boot/sbl_prebuilt/am273x-evm all: ifeq ($(CCS_IDE_MODE),cloud) # No post build steps else @echo Boot image: am273x:r5fss0-0:nortos:ti-arm-clang $(BOOTIMAGE_NAME) ... $(OBJCOPY) --strip-all -O binary $(OUTFILE) $(BOOTIMAGE_BIN_NAME) ifeq ($(DEVICE_TYPE),HS) ifeq ($(DEBUG_TIFS), yes) ifeq ($(ENC_SBL_ENABLED),yes) $(BOOTIMAGE_CERT_GEN_CMD) --sbl-enc --enc-key $(APP_ENCRYPTION_KEY) --image-bin $(BOOTIMAGE_BIN_NAME) --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key $(BOOTIMAGE_CERT_KEY) --kd-salt $(KD_SALT) --out-image $(BOOTIMAGE_NAME) else $(BOOTIMAGE_CERT_GEN_CMD) --image-bin $(BOOTIMAGE_BIN_NAME) --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key $(BOOTIMAGE_CERT_KEY) --out-image $(BOOTIMAGE_NAME) endif else ifeq ($(ENC_SBL_ENABLED),yes) $(BOOTIMAGE_CERT_GEN_CMD) --sbl-enc --enc-key $(APP_ENCRYPTION_KEY) --image-bin $(BOOTIMAGE_BIN_NAME) --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key $(BOOTIMAGE_CERT_KEY) --kd-salt $(KD_SALT) --out-image $(BOOTIMAGE_NAME) --debug $(DEBUG_OPTION) else $(BOOTIMAGE_CERT_GEN_CMD) --image-bin $(BOOTIMAGE_BIN_NAME) --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key $(BOOTIMAGE_CERT_KEY) --out-image $(BOOTIMAGE_NAME) --debug $(DEBUG_OPTION) endif endif else $(BOOTIMAGE_CERT_GEN_CMD) --image-bin $(BOOTIMAGE_BIN_NAME) --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key $(BOOTIMAGE_CERT_KEY) --out-image $(BOOTIMAGE_NAME) --debug DBG_SOC_DEFAULT @echo Boot image: am273x:r5fss0-0:nortos:ti-arm-clang $(BOOTIMAGE_NAME) Done !!! @echo . endif endif
Can this example apply to my project?