Part Number: TMS570LS1224
Hi,
I need to implement an MCU reset (warm/cold) upon an ESM error.
In this regard, could anyone please advise:
1. If there is some recommended schematic (or least voltage monitor part numbers) that could be used accordingly - maybe in a loop-back from the nERROR pin to the nRST and nPORRST?
2. Or could it be done internally - as part of an ISR, or even via some lower level "multiplexer" circuitry inside the Hercules?
Thanks,
Varban