Part Number: MSPM0L1305
Other Parts Discussed in Thread: BQ76952
Hi,
Background:
I am currently working with a custom board that features an MSPM0L1305 as the main MCU, communicating with two BQ76952 chips via I2C. Upon resetting the MCU, I sometimes observe the I2C bus getting stuck low, causing the program to hang indefinitely while waiting to exit the "bus busy" state. The I2C bus only recovers when I completely reset the BQ76952 chips by disconnecting and reconnecting the power.
Question:
Is there any way the host MCU can inform the targets (BQ76952) to release the bus in this situation?
I was informed that the controller generating 9-10 scl cycles will do the trick. If this is a recommended solution, can you please provide the correct way to generate a certain number of clock cycles?
Thank you,
Kyungjae Lee