Part Number: AM2634
Tool/software:
environment: CCS12.7 sdk9.0.02 demo: adc_multiple_soc_epwm_am263x-lp-nortos hardware: 2634lp red demo board
When I first ran the example program and it worked properly, I could see the ADC value. With nothing changed, I ran the example again,(right click AM263x.ccxml->debug->CPU reset->load program->choose project->run)
The code stop at line 115 in adc_multiple_soc_epwm.c
/* Wait until required number of ADC conversions are completed */
while( gAdcConversionCount < ADC_CONVERSION_COUNT );
can see "[Cortex_R5_0] ADC EPWM Triggered Conversion Test Started ..."in console and no ADC value.
Must power off the board then the example program can work properly, why?