Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I'm trying to setup the pin mappings in SysConfig according to the schematic from my EE. However, I cannot select PA5 (pin 9) or PA10 (pin 14) as GPIO pins. They simply don't appear in the list of pins. I have checked that I do not have either of those pins assigned to anything else. Additionally, the device pin diagram in SysConfig shows those two pins as available.


I've attached the generated pin assignments text file from SysConfig.
- GPIOA: + Open-Drain Output: PA0 + Standard Output: PA26 + Standard Input: PA16 + Standard Input: PA15 + Standard Input: PA22 + Standard Input: PA2 + Standard Input: PA3 + Standard Input: PA4 + Standard Input: PA14 + Standard Input: PA6 + Standard Input: PA7 + Standard Input: PA13 + Standard Input: PA11 + Standard Input: PA12 - SYSCTL - UART0: + RX Pin: PA9 + TX Pin: PA8 - EVENT - CRC - SYSTICK - WWDT0 - BOARD: + Debug Clock: PA20 + Debug Data In Out: PA19