Part Number: TMS570LC4357
Tool/software:
Hi,
I'm trying to measure the internal temperature on TMS570LC43, I'm using a reference voltage of 3.3V and the example code from TI Application note SPNA216. I think I'm having problems with calibration because I'm getting Junction temperatures above 78°C in an aprox 22°C ambient temperature.
My results from calibration are:
offset = 102.0214
slope = 0.16675
These results make sense? I don't know if maybe there is a wrong configuration in the ADC driver. I'm using the default values with ADC2 Group1 discharge time of 500ns and Sample time of 1us.
Thank you!
Best regards,