Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG,
Tool/software:
I have an existing project using the MSPM0 SDK and GCC in CCS Theia. I want to switch it to use TI Clang instead. However, after I changed the Compiler in the Project General properties, the build now fails with an error from SysConfig:
[10]**** Build of configuration Debug-Launchpad__TICLANG for project MotionLogicController ****
[11]"C:\\ti\\ccstheia140\\ccs\\utils\\bin\\gmake" -k -j 16 all -O
[12]Building file: "../mspm0l1306_launchpad.syscfg"
[13]Invoking: SysConfig
[14]"C:/ti/ccstheia140/ccs/utils/sysconfig_1.20.0/sysconfig_cli.bat" --script "C:/Users/gordon.tyler/workspace_ccstheia/MotionLogicController/mspm0l1306_launchpad.syscfg" -o "syscfg" --compiler ticlang
[15]Usage:
[16] cli [-o <dir>] [-s <file>] [-u <string>] [-b <name>] [-d <name>] [-p <name>] [-r <name>] [--treatWarningsAsErrors] [--quiet -q] <script>
[17] cli --help
[18] cli --version
[19] example: cli -s meta_data/sdk.json -d MSP432P401R scripts/two_uarts.js
[20] example: -s sdk.json -d MSP432P401R -o ./display_cfg sdk/cfgs/display.syscfg
[21] Note that the all arguments other than '--help' and '--version' may also be
[22] specified via the script with an embedded @cliArgs comment directive.
[23] E.g. // @cliArgs -d MSP432P401R
[24] If an argument is embedded in a script and explicitly specified via the CLI
[25] then precedence is given to the CLI arguments. Additionally, specifying
[26] "--board" or "--device" on the CLI will override any "--board" and "--device"
[27] arguments specified in the script.
[28]subdir_rules.mk:16: recipe for target 'build-763525025' failed
[29]Invalid argument '--product': No product with name "mspm0_sdk" and version "2.00.01.01" found
It looks like the Product Dependencies for the MSPM0 SDK and SysConfig were not added to the new build configuration created when I switch the compiler. However, after re-adding these dependencies, the build still fails at the SysConfig step:
[10]**** Build of configuration Debug-Launchpad__TICLANG for project MotionLogicController ****
[11]"C:\\ti\\ccstheia140\\ccs\\utils\\bin\\gmake" -k -j 16 all -O
[12]Building file: "../mspm0l1306_launchpad.syscfg"
[13]Invoking: SysConfig
[14]"C:/ti/ccstheia140/ccs/utils/sysconfig_1.20.0/sysconfig_cli.bat" --script "C:/Users/gordon.tyler/workspace_ccstheia/MotionLogicController/mspm0l1306_launchpad.syscfg" -o "syscfg" -s "C:/ti/simplelink_msp432e4_sdk_4_20_00_12/.metadata/product.json" --compiler ticlang
[15]Usage:
[16] cli [-o <dir>] [-s <file>] [-u <string>] [-b <name>] [-d <name>] [-p <name>] [-r <name>] [--treatWarningsAsErrors] [--quiet -q] <script>
[17] cli --help
[18] cli --version
[19] example: cli -s meta_data/sdk.json -d MSP432P401R scripts/two_uarts.js
[20] example: -s sdk.json -d MSP432P401R -o ./display_cfg sdk/cfgs/display.syscfg
[21] Note that the all arguments other than '--help' and '--version' may also be
[22] specified via the script with an embedded @cliArgs comment directive.
[23] E.g. // @cliArgs -d MSP432P401R
[24] If an argument is embedded in a script and explicitly specified via the CLI
[25] then precedence is given to the CLI arguments. Additionally, specifying
[26] "--board" or "--device" on the CLI will override any "--board" and "--device"
[27] arguments specified in the script.
[28]subdir_rules.mk:16: recipe for target 'build-763525025' failed
[29]/ti/boards/LP_MSPM0L1306: No such resource: /ti/boards/LP_MSPM0L1306.syscfg.json
[30]Paths searched:
[31]C:\ti\simplelink_msp432e4_sdk_4_20_00_12\source\ti\boards\LP_MSPM0L1306.syscfg.json
[32]C:\ti\simplelink_msp432e4_sdk_4_20_00_12\source\ti\boards\.meta\LP_MSPM0L1306.syscfg.json
[33]C:\ti\simplelink_msp432e4_sdk_4_20_00_12\source\ti\.meta\boards\LP_MSPM0L1306.syscfg.json
[34]C:\ti\simplelink_msp432e4_sdk_4_20_00_12\source\.meta\ti\boards\LP_MSPM0L1306.syscfg.json
[35]C:\Users\gordon.tyler\workspace_ccstheia\MotionLogicController\ti\boards\LP_MSPM0L1306.syscfg.json
[36]C:\Users\gordon.tyler\workspace_ccstheia\MotionLogicController\ti\boards\.meta\LP_MSPM0L1306.syscfg.json
[37]C:\Users\gordon.tyler\workspace_ccstheia\MotionLogicController\ti\.meta\boards\LP_MSPM0L1306.syscfg.json
[38]C:\Users\gordon.tyler\workspace_ccstheia\MotionLogicController\.meta\ti\boards\LP_MSPM0L1306.syscfg.json
What adjustments do I need to make to the project configuration to get it working again?