Part Number: MSP-EXP432E401Y
Tool/software:
/* --COPYRIGHT--,BSD
* Copyright (c) 2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
/******************************************************************************
* MSP432E4 example code for CMSIS DSP Library.
*
* Description: The ADC is configured to sample AIN0 channel using a timer
* trigger at 100 KHz. The DMA is configured to transfer the data from the ADC
* to SRAM buffer using Ping-Pong mechanism. When the data buffer is copied the
* ADC gives a DMA Done interrupt to which the CPU first re-initializes the DMA
* and the performs sample-averaging for DC value, RMS calculation and FFT of
* the data and displays on the serial console the DC average, RMS, maximum
* FFT energy and FFT frequency bin at which maximum energy is detected.
*
* CMSIS DSP Function Used:
* 1. arm_sqrt_f32
* 2. arm_cfft_q15
* 3. arm_cmplx_mag_q15
* 4. arm_max_q15
*
* MSP432E401Y
* ------------------
* /|\| |
* | | |
* --|RST PE3|<--AIN0
* | |
* | |
* | |
* | PA0|<--U0RX
* | PA1|-->U0TX
* Author: Amit Ashara
*******************************************************************************/
/* DriverLib Includes */
#include <ti/devices/msp432e4/driverlib/driverlib.h>
/* Standard Includes */
#include <stdint.h>
#include <stdbool.h>
/* Display Include via console */
#include "uartstdio.h"
#include "arm_math.h"
#include "arm_const_structs.h"
/* Define for Samples to be captured and Sampling Frequency */
#define NUM_SAMPLES 1024
#define SAMP_FREQ 100000
/* DMA Buffer declaration and buffer complet flag */
static uint32_t dstBufferA[NUM_SAMPLES];
static uint32_t dstBufferB[NUM_SAMPLES];
volatile bool setBufAReady = false;
volatile bool setBufBReady = false;
/* Global variables and defines for FFT */
#define IFFTFLAG 0
#define BITREVERSE 1
volatile int16_t fftOutput[NUM_SAMPLES*2];
/* Global variables for RMS and DC calculation */
volatile float32_t rmsBuff;
volatile float32_t dcBuff;
float32_t rmsCalculation;
/* The control table used by the uDMA controller. This table must be aligned
* to a 1024 byte boundary. */
#if defined(__ICCARM__)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(__TI_ARM__)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
void ADC0SS2_IRQHandler(void)
{
uint32_t getIntStatus;
uint32_t getDMAStatus;
/* Get the interrupt status from the ADC */
getIntStatus = MAP_ADCIntStatusEx(ADC0_BASE, true);
/* Clear the ADC interrupt flag. */
MAP_ADCIntClearEx(ADC0_BASE, getIntStatus);
/* Read the primary and alternate control structures to find out which
* of the structure has completed and generated the done interrupt. Then
* re-initialize the appropriate structure */
getDMAStatus = MAP_uDMAChannelModeGet(UDMA_CH16_ADC0_2 |
UDMA_PRI_SELECT);
/* Check if the primary or alternate channel has completed. On completion
* re-initalize the channel control structure. If the Primary channel has
* completed then set Buffer-A ready flag so that the main application
* may perform the DSP computation. Similarly if the Alternate channel
* has completed then set Buffer-B ready flag so that the main application
* may perform the DSP computation. */
if(getDMAStatus == UDMA_MODE_STOP)
{
MAP_uDMAChannelTransferSet(UDMA_CH16_ADC0_2 | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)&ADC0->SSFIFO2, (void *)&dstBufferA,
sizeof(dstBufferA)/4);
setBufAReady = true;
}
getDMAStatus = MAP_uDMAChannelModeGet(UDMA_CH16_ADC0_2 |
UDMA_ALT_SELECT);
if(getDMAStatus == UDMA_MODE_STOP)
{
MAP_uDMAChannelTransferSet(UDMA_CH16_ADC0_2 | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)&ADC0->SSFIFO2, (void *)&dstBufferB,
sizeof(dstBufferB)/4);
setBufBReady = true;
}
}
void ConfigureUART(uint32_t systemClock)
{
/* Enable the clock to GPIO port A and UART 0 */
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
/* Configure the GPIO Port A for UART 0 */
MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
/* Configure the UART for 115200 bps 8-N-1 format */
UARTStdioConfig(0, 115200, systemClock);
}
int main(void)
{
uint32_t systemClock;
uint32_t ii;
uint32_t setFFTmaxValue;
uint32_t setFFTmaxFreqIndex;
int_fast32_t i32IPart[3];
int_fast32_t i32FPart[3];
/* Configure the system clock for 120 MHz */
systemClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
/* Initialize serial console */
ConfigureUART(systemClock);
/* Display the setup on the console. */
/*UARTprintf("\033[2J\033[H");
UARTprintf("\rCMSIS DSP Demo...\n\n");
UARTprintf("\033[2GDC Average \033[31G\n");
UARTprintf("\033[2GRMS \033[31G\n");
UARTprintf("\033[2GFFT Amplitude \033[31G\n");
UARTprintf("\033[2GFFT Frequency \033[31G\n");
*/
/* Enable the clock to GPIO Port E and wait for it to be ready */
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE)))
{
}
/* Configure PE3 as ADC input channel */
MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
/* Enable the clock to ADC-0 and wait for it to be ready */
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0)))
{
}
/* Configure Sequencer 2 to sample the analog channel : AIN0. The end of
* conversion and interrupt generation is set for AIN0 */
MAP_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH0 | ADC_CTL_IE |
ADC_CTL_END);
/* Enable sample sequence 2 with a timer signal trigger. Sequencer 2
* will do a single sample when the timer generates a trigger on timeout*/
MAP_ADCSequenceConfigure(ADC0_BASE, 2, ADC_TRIGGER_TIMER, 2);
/* Clear the interrupt status flag before enabling. This is done to make
* sure the interrupt flag is cleared before we sample. */
MAP_ADCIntClearEx(ADC0_BASE, ADC_INT_DMA_SS2);
MAP_ADCIntEnableEx(ADC0_BASE, ADC_INT_DMA_SS2);
/* Enable the DMA request from ADC0 Sequencer 2 */
MAP_ADCSequenceDMAEnable(ADC0_BASE, 2);
/* Since sample sequence 2 is now configured, it must be enabled. */
MAP_ADCSequenceEnable(ADC0_BASE, 2);
/* Enable the Interrupt generation from the ADC-0 Sequencer */
MAP_IntEnable(INT_ADC0SS2);
/* Enable the DMA and Configure Channel for TIMER0A for Ping Pong mode of
* transfer */
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_UDMA)))
{
}
MAP_uDMAEnable();
/* Point at the control table to use for channel control structures. */
MAP_uDMAControlBaseSet(pui8ControlTable);
/* Map the ADC0 Sequencer 2 DMA channel */
MAP_uDMAChannelAssign(UDMA_CH16_ADC0_2);
/* Put the attributes in a known state for the uDMA ADC0 Sequencer 2
* channel. These should already be disabled by default. */
MAP_uDMAChannelAttributeDisable(UDMA_CH16_ADC0_2,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
/* Configure the control parameters for the primary control structure for
* the ADC0 Sequencer 2 channel. The primary control structure is used for
* copying the data from ADC0 Sequencer 2 FIFO to dstBufferA. The transfer
* data size is 32 bits and the source address is not incremented while
* the destination address is incremented at 32-bit boundary.
*/
MAP_uDMAChannelControlSet(UDMA_CH16_ADC0_2 | UDMA_PRI_SELECT,
UDMA_SIZE_32 | UDMA_SRC_INC_NONE |
UDMA_DST_INC_32 | UDMA_ARB_1);
/* Set up the transfer parameters for the ADC0 Sequencer 2 primary control
* structure. The mode is Basic mode so it will run to completion. */
MAP_uDMAChannelTransferSet(UDMA_CH16_ADC0_2 | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)&ADC0->SSFIFO2, (void *)&dstBufferA,
sizeof(dstBufferA)/4);
/* Configure the control parameters for the alternate control structure for
* the ADC0 Sequencer 2 channel. The alternate control structure is used for
* copying the data from ADC0 Sequencer 2 FIFO to dstBufferB. The transfer
* data size is 32 bits and the source address is not incremented while
* the destination address is incremented at 32-bit boundary.
*/
MAP_uDMAChannelControlSet(UDMA_CH16_ADC0_2 | UDMA_ALT_SELECT,
UDMA_SIZE_32 | UDMA_SRC_INC_NONE |
UDMA_DST_INC_32 | UDMA_ARB_1);
/* Set up the transfer parameters for the ADC0 Sequencer 2 alternate
* control structure. The mode is Basic mode so it will run to
* completion */
MAP_uDMAChannelTransferSet(UDMA_CH16_ADC0_2 | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)&ADC0->SSFIFO2, (void *)&dstBufferB,
sizeof(dstBufferB)/4);
/* The uDMA ADC0 Sequencer 2 channel is primed to start a transfer. As
* soon as the channel is enabled and the Timer will issue an ADC trigger,
* the ADC will perform the conversion and send a DMA Request. The data
* transfers will begin. */
MAP_uDMAChannelEnable(UDMA_CH16_ADC0_2);
/* Enable Timer-0 clock and configure the timer in periodic mode with
* a frequency of 1 KHz. Enable the ADC trigger generation from the
* timer-0. */
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER0)))
{
}
MAP_TimerConfigure(TIMER0_BASE, TIMER_CFG_A_PERIODIC);
MAP_TimerLoadSet(TIMER0_BASE, TIMER_A, (systemClock/SAMP_FREQ));
MAP_TimerADCEventSet(TIMER0_BASE, TIMER_ADC_TIMEOUT_A);
MAP_TimerControlTrigger(TIMER0_BASE, TIMER_A, true);
MAP_TimerEnable(TIMER0_BASE, TIMER_A);
/* While loop to process the data */
while(1)
{
/* Wait for Primary channel to complete and then clear the flag and
* initialize the variables */
while(!setBufAReady);
setBufAReady = false;
dcBuff = 0.0f;
rmsBuff = 0.0f;
/* First convert the sampled data to floating point format as the RMS
* and DC average is being computed */
for(ii=0;ii<NUM_SAMPLES;ii++)
{
rmsBuff += ((float32_t)(dstBufferA[ii]*dstBufferA[ii])*(float32_t)(33*33))/(float32_t)(40960*40960);
dcBuff += (float32_t)(dstBufferA[ii]*33)/(float32_t)40960;
}
/* Now calculate the final DC Average and RMS */
dcBuff = dcBuff/((float32_t)NUM_SAMPLES);
rmsBuff = rmsBuff/((float32_t)NUM_SAMPLES);
arm_sqrt_f32(rmsBuff,&rmsCalculation);
/* Compute the 1024 point FFT on the sampled data and then find the
* FFT point for maximum energy and the energy value */
arm_cfft_q15(&arm_cfft_sR_q15_len1024, (q15_t *)dstBufferA, IFFTFLAG,
BITREVERSE);
arm_cmplx_mag_q15((q15_t *)dstBufferA, (q15_t *)fftOutput,
NUM_SAMPLES);
arm_max_q15((q15_t *)fftOutput, NUM_SAMPLES, (q15_t *)&setFFTmaxValue,
&setFFTmaxFreqIndex);
/* Convert the floating point values to integer and fractional parts
* for display on the serial console */
i32IPart[0] = (int32_t) rmsCalculation;
i32FPart[0] = (int32_t) (rmsCalculation*1000.0f);
i32FPart[0] = (int32_t)(i32FPart[0] - i32IPart[0]*1000.0);
i32IPart[1] = (int32_t) dcBuff;
i32FPart[1] = (int32_t) (dcBuff*1000.0f);
i32FPart[1] = (int32_t)(i32FPart[1] - i32IPart[1]*1000.0);
i32IPart[2] = (int32_t) ((setFFTmaxFreqIndex*SAMP_FREQ)/NUM_SAMPLES);
i32FPart[2] = (int32_t) (((setFFTmaxFreqIndex*SAMP_FREQ)/NUM_SAMPLES)*1000);
i32FPart[2] = i32FPart[2] - i32IPart[2]*1000;
/* Print the DC Average, RMS, Maximum FFT Amplitude and the FFT
* frequency at which Max FFT Amplitude is detected */
UARTprintf("\033[3;17H%3d.%03d Volts\n", i32IPart[0], i32FPart[0]);
UARTprintf("\033[4;17H%3d.%03d Volts\n", i32IPart[1], i32FPart[1]);
UARTprintf("\033[5;19H%03d\n", setFFTmaxValue);
UARTprintf("\033[6;17H%3d.%03d Hz\n", i32IPart[2], i32FPart[2]);
/* Wait for Alternate channel to complete and then clear the flag and
* initialize the variables */
while(!setBufBReady);
setBufBReady = false;
dcBuff = 0.0f;
rmsBuff = 0.0f;
/* First convert the sampled data to floating point format as the RMS
* and DC average is being computed */
for(ii=0;ii<NUM_SAMPLES;ii++)
{
rmsBuff += ((float32_t)(dstBufferB[ii]*dstBufferB[ii])*(float32_t)(33*33))/(float32_t)(40960*40960);
dcBuff += (float32_t)(dstBufferB[ii]*33)/(float32_t)40960;
}
/* Now calculate the final DC Average and RMS */
dcBuff = dcBuff/((float32_t)NUM_SAMPLES);
rmsBuff = rmsBuff/((float32_t)NUM_SAMPLES);
arm_sqrt_f32(rmsBuff,&rmsCalculation);
/* Compute the 1024 point FFT on the sampled data and then find the
* FFT point for maximum energy and the energy value */
arm_cfft_q15(&arm_cfft_sR_q15_len1024, (q15_t *)dstBufferB, IFFTFLAG,
BITREVERSE);
arm_cmplx_mag_q15((q15_t *)dstBufferB, (q15_t *)fftOutput,
NUM_SAMPLES);
arm_max_q15((q15_t *)fftOutput, NUM_SAMPLES, (q15_t *)&setFFTmaxValue,
&setFFTmaxFreqIndex);
/* Convert the floating point values to integer and fractional parts
* for display on the serial console */
i32IPart[0] = (int32_t) rmsCalculation;
i32FPart[0] = (int32_t) (rmsCalculation*1000.0f);
i32FPart[0] = (int32_t)(i32FPart[0] - i32IPart[0]*1000.0);
i32IPart[1] = (int32_t) dcBuff;
i32FPart[1] = (int32_t) (dcBuff*1000.0f);
i32FPart[1] = (int32_t)(i32FPart[1] - i32IPart[1]*1000.0);
i32IPart[2] = (int32_t) ((setFFTmaxFreqIndex*SAMP_FREQ)/NUM_SAMPLES);
i32FPart[2] = (int32_t) (((setFFTmaxFreqIndex*SAMP_FREQ)/NUM_SAMPLES)*1000);
i32FPart[2] = i32FPart[2] - i32IPart[2]*1000;
/* Print the DC Average, RMS, Maximum FFT Amplitude and the FFT
* frequency at which Max FFT Amplitude is detected */
UARTprintf("\033[3;17H%3d.%03d\n", i32IPart[0], i32FPart[0]);
UARTprintf("\033[4;17H%3d.%03d\n", i32IPart[1], i32FPart[1]);
UARTprintf("\033[5;19H%03d\n", setFFTmaxValue);
UARTprintf("\033[6;17H%3d.%03d Hz\n", i32IPart[2], i32FPart[2]);
}
}
Hello,
I am working on integration of ADXL1002Z sensor to EXP432E401Y dev.kit. Using CMSIS_MSP432e4_dsp example, I am getting FFT amplitude and frequency value. But the values are keep on fluctuating even the sensor position is stable.
Is the attached code can be used for computation of FFT of analog signal or any changes to be done to the code. kindly help with this issue. Before going for calibration, i would like to confirm whether the FFT readings are reliable or not. It would be great, if you can guide me with working code to compute the FFT of accelerometer signal using MSP432E4 MCU. Any reference to understand the code will be helpful.
Thank you
Links---