This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: USB0VBUS

Part Number: TM4C129ENCPDT

Tool/software:

USB0VBUS is 5V voltage, but can 5V from USB0VBUS flow to VCC (3.3V) line in TM4C129ENCPDT?
When 3.3V voltage is not supplied to VCC, if USB cable is connected and 5V is supplied to USB0VBUS, 3.3V voltage rises to about 0.05V or 1V.
Do you know the cause of the above?

  • Hi,

    USB0VBUS is 5V voltage, but can 5V from USB0VBUS flow to VCC (3.3V) line in TM4C129ENCPDT?
    When 3.3V voltage is not supplied to VCC, if USB cable is connected and 5V is supplied to USB0VBUS, 3.3V voltage rises to about 0.05V or 1V.
    Do you know the cause of the above?

    Please refer to the datasheet for details about the limit on the IO pad voltage when the device is unpowered. 

    Also refer to the TM4C129 System Design Guideline for best practice on VBUS signal. A 100ohm series resistor is recommended if you plan to use only in USB Device mode.