This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: Error initializing flash programming: using XDS200

Part Number: TMS570LS3137

Tool/software:

Hello, 

I've been using XDS200 debuger for TMS570LS3137 for quite some time.

However recently we made some changes to the linker command file, since then we face following error message while trying to debug:(in Code composer studio 12.1.0)

CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: Error initializing flash programming: Target failed to read 0xFFFFFFF0
CortexR4: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
CortexR4: File Loader: Verification failed: Values at address 0x00000000 do not match Please verify target memory and memory map.
CortexR4: GEL: File: C:\Workspace\Dev\src\safetyBms_prototype\build\SafetyBmsPrototype.out: a data verification error occurred, file load failed."

I went through the forum to debug and followed the advice of verifying the linker file etc.. everything seems "fine". 

I also notice that XDS200 seems to work well with completely erase flash.(erase operation done with segger Jlink).

Highly appreciate your response.

Best Regards,

Anudeep Varada