Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Format/ scaling factor for estimatedSpeed in sensorless FOC example

Part Number: MSPM0G3507

Tool/software:

Hello,

I'm trying to get the DAC12 to output the estimated speed as its output value in the sensorless FOC example with DRV8323RS. I'm running this based on the latest SDK of 02.00.01.

I have set the dacOutAddr to the correct value (it does not match the tuning guide, but validated through expression window), and dac output is enabled, but what I'm seeing is basically periodic pulses instead of the voltage ramping as the motor accelerates:

For reference this is what the rest of my outputs look like over the course of the recording:

I see that in the tuning guide there are tips for adjusting the scaling factor based on the number format, but if I look at the estimated speed parameter it's just defined as int32_t. What are the units and what is the Q format for this number?

Munan