Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Configuration for unused pins

Part Number: MSPM0G3507

Tool/software:

Hi TI,

Currently I am referring the MSPM0G3507 datasheet. In that it is mentioned about unused pins. see the below image.

Example:

1. I am using only Port A pins from 1 to 10(PA0 - PA10) and not using other pins. So do I need to configure unused pins as GPIO and set the pins as output low or input pullup/pull down as mentioned in datasheet. 

or I can configure the unused pins with default configuration which is 0x0000 0000 for PINCMx register. what do you suggest?

Thanks.