Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello all,
we use the internal SYSOSC and the SYSPLL to generate 80MHz for MCLK and CPUCLK:
DL_SYSCTL_SYSPLLConfig gSYSPLLConfig;
gSYSPLLConfig.rDivClk2x = 1;
gSYSPLLConfig.rDivClk1 = 0;
gSYSPLLConfig.rDivClk0 = 0;
gSYSPLLConfig.enableCLK2x = DL_SYSCTL_SYSPLL_CLK2X_ENABLE;
gSYSPLLConfig.enableCLK1 = DL_SYSCTL_SYSPLL_CLK1_DISABLE;
gSYSPLLConfig.enableCLK0 = DL_SYSCTL_SYSPLL_CLK0_DISABLE;
gSYSPLLConfig.sysPLLMCLK = DL_SYSCTL_SYSPLL_MCLK_CLK2X;
gSYSPLLConfig.sysPLLRef = DL_SYSCTL_SYSPLL_REF_SYSOSC;
gSYSPLLConfig.qDiv = 4;
gSYSPLLConfig.pDiv = DL_SYSCTL_SYSPLL_PDIV_2;
gSYSPLLConfig.inputFreq = DL_SYSCTL_SYSPLL_INPUT_FREQ_16_32_MHZ;
/* SYSOSC / PDIV * QDIV = 32MHz / 2 * 5 = 80MHz */
DL_SYSCTL_configSYSPLL((DL_SYSCTL_SYSPLLConfig *)&gSYSPLLConfig);
DL_SYSCTL_setULPCLKDivider(DL_SYSCTL_ULPCLK_DIV_2);
DL_SYSCTL_switchMCLKfromSYSOSCtoHSCLK(DL_SYSCTL_HSCLK_SOURCE_SYSPLL);
// With MCLK=80MHz 2 flash wait states are required
// For details see datasheet section 7.3 Recommended Operating Conditions
DL_SYSCTL_setFlashWaitState(DL_SYSCTL_FLASH_WAIT_STATE_2);
while ((DL_SYSCTL_getClockStatus() & DL_SYSCTL_CLK_STATUS_SYSPLL_GOOD) !=
DL_SYSCTL_CLK_STATUS_SYSPLL_GOOD) {
;
}
This works approximately 9 out 10 power-ups fine, but one time the PLL output frequency seems to be wrong for the whole operation cycle. In the faulty cases I measured 72.8MHz or 39.5MHz instead of the expected 80Mhz. I tested on two different hardwares and failure occurs on both (with different faulty frequencies though).
With above configuration VCO frequency is 80Mhz (valid range according to data sheet 60...400MHz) and SYSPLLCLK2X output frequency also 80MHz (valid range according to data sheet 4...800MHz). In my opinion this is a valid configuration, also the TI tool SysConfig does not show any warnings or errors and I saw that these values are used as example in the RM.
However, I noticed that with a following different PLL configuration the issue seems not occurring:
gSYSPLLConfig.rDivClk2x = 3;
gSYSPLLConfig.qDiv = 9;
With qDIV = x10 VCO frequency is 160MHz and CLK2X_DIV = 4, the PLL output frequency is 80MHz as in above configuration. I tested 250 power-up cycles without any wrong frequency.
Currently we use MSPM0 SDK 1.20.1.6 (I did not notice relevant changes in sysctl in SDK version 2.00.01.00).
Do you see an issue with the used initialization sequence of the clock configuration?
Is there a known issue in the driver lib?
If not, could you please try to reproduce this issue?
Thank you in advance!
Best regards,
Holger