This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNIFLASH: Error -1066 after load image

Part Number: UNIFLASH
Other Parts Discussed in Thread: CC2340R5, LP-XDS110,

Tool/software:

Hi,

I am using CC2340R5 with LP-XDS110, the environment is Ubuntu 24.04.

After flash the images by UniFlash 8.7, there is always Error -1066 in console log.

I want to know what is the cause? and whether there will be any impact

[2024/6/12 上午10:03:01] [INFO] Cortex_M0P: Updating CRC32 field ccfg.bootCfg.crc32 @ address 0x4E02000C, based on data in the range [0x4E020000, 0x4E02000B]. Value changes from 0x00000000 to 0xFFFFFFFF
[2024/6/12 上午10:03:01] [INFO] Cortex_M0P: Updating CRC32 field ccfg.crc32 @ address 0x4E02074C, based on data in the range [0x4E020010, 0x4E02074B]. Value changes from 0x00000000 to 0x915ECEFA
[2024/6/12 上午10:03:01] [INFO] Cortex_M0P: Updating CRC32 field ccfg.debugCfg.crc32 @ address 0x4E0207FC, based on data in the range [0x4E0207D0, 0x4E0207FB]. Value changes from 0x00000000 to 0x527294A2
[2024/6/12 上午10:03:02] [INFO] Cortex_M0P: GEL Output: Memory Map Initialization Complete.
[2024/6/12 上午10:03:02] [ERROR] Cortex_M0P: Trouble Setting Breakpoint with the Action "Terminate GEL_Go()" at 0xf0023f1: (Error -1066 @ 0xF0023F0) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 12.7.0.00130)
[2024/6/12 上午10:03:02] [ERROR] Cortex_M0P: GEL: Error while executing OnTargetConnect(): An earlier error prevented the target from running at GEL_Go(entryPoint) [cc23xx_xds.gel:55] at OnTargetConnect()
[2024/6/12 上午10:03:02] [SUCCESS] Program Load completed successfully.

Thanks

8358.ds.log