Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Tool/software:
Hello Everyone,
I'm trying to flash an MSPM0L1306 that I've installed on a custom board. At this point I'm just trying to flash it with an empty file and I keep getting this message
Error connecting to the target: (Error -6305) PRSC module failed to write to a router register. (Emulation package 12.7.0.00130)
To flash the board I'm using a MSPM03507 Launchpad's XDS110 debugger headers. I'm not powering the board at all, rather I'm powering it through the debugger. The pins I have connected are 3.3V, GND, BSL, SWDIO,SCLK, NRST. I'm using CCS Theia vs 1.4.0 and with the empty_mspm0l1306 example project. I've made sure to go into the Sysconfig Device manager and switch the package to the SOT-16(DYY) that I have on my board.
Do you have any tips on getting the IC to flash?
Thanks,
Robert